This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65100: Doubler or Trippler?

Part Number: TPS65100


Our design calls for a VGH = 18V.  This would correspond to Vo3 = 18V.  The question is do I use the Doubler configuration or Trippler configuration?  In the Doubler configuration, the max Vo3 indicated on page 22 of the data sheet calls for 2xVo1 - (2xVf+2xIo(2xrdsonQ5 + rdsonQ3 +rdsonQ4)).

My Vo1 = 10V.

When using the equation with the given rdsON values, I get around 17.8V typical and 17.2V for max rdsON values.  This math would make me consider using the Trippler mode.  I cannot find where the minimum Vo3 is in Trippler mode in the data sheet, but everything on these forums say it's min is 2xVo1 = 20V.  The question then becomes, if I can't get Vo3 = 18V in Doubler mode because of the rdsOn losses, and the min for Trippler mode is too high (2xVo1 = 20V), which mode do I use?

Thanks,

Kevin