Hello,
I would just like to confirm my understanding of a datasheet spec. I am using the REF3212 in an application that is expected to experience lightning strikes and want to make sure the REF3121 can handle the brief high voltage and current on the OUT_F and OUT_S pins. I've attached a screenshot of my circuit.
In the datasheet, there is no specific max rating on the OUT_F and OUT_S pins in the "Absolute Maximum Ratings" section so I'm assuming these pins can handle only +7.5 voltage maximums which is placed on the "Input Voltage". Also, what is the maximum current that the Vo pins can handle? 40mA per the Isc sinking spec?
Thanks,
Hayden