This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Arria 10 GX320 PMIC reference design

Other Parts Discussed in Thread: TPS650861, TPS53647, TPS548D22, TPS54618, TPS53515, TPS54418, TPS65251, TPS65262-2

Hello,

Customer is looking for referenced PMIC for Arria 10 GX320.

Does TI have reference PMIC? Only can find below post.

Please let me get Reference Power design for Arria 10 GX320.

Regards, 

Nicky

Technical solutions, industry trends and insights for designing and managing your power supplies.
0 posts

  • Hi Nicky,

    [2020 Edit: The TPS650861 is the user programmable version of TPS650860 which can be programmed for a wide variety of cases and is an excellent option for FPGA attach with a wide variety of current]

    We don't have a PMIC reference design for the Arria 10 family. There is a very wide range of use cases and no single solution tends to work for multiple opportunities. The most promising was the use of the TPS650860 with an MSP430 to set the voltages during boot and then enable rails by I2C. Rail mapping will vary based on how much current is desired from each.

    If you have any power tree we can help to identify if there is a good PMIC fit.

  • Hi Kevin,

    If there is no PMIC solution, customer wants to use attached TI Switching Regulator Power Proposal. (see attached.)

    But those  parts are too heavy to use customer's solution, so she wants to get new proposal as below table.

    Could you recommend a little light solutions?

    Arria 10 10AX016E1F27 Power Tree
    Power Up   Recommend New Ti Part NET Name Arria 10 VCC Arria 10 Voltage Current (A) TI Proposed Part
    1st     A10_VCC VCC_VCCP 0.9V 3.6015 TPS53647 12V
    Vin Max = 45 ~ 50V
    (Vin = 30V)
      A10_VCCRT_GXB VCCRT_GXB 1.03V 2.634 TPS5353 TPS548D22
      A10_VCCRAM VCCERAM 0.95V 0.0645 TPS54618
    2nd   A10_1.8V VCCA_PLL, VCCH_GXB 1.8V 1.2315 TPS53515
      A10_VCCPT VCCPT, VCCBAT 1.8V 0.456
    3rd       3.0V (Only on 3.0V I/O Bank)    
          2.5V (Only on 3.0V I/O Bank)    
      A10_VCCIO_1.8V VCCIO_1.8V, VCCPGM, VREFP/N_ADC 1.8V 0.075 TPS54618
      A10_VCCIO_MEM VCCIO_MEM & MEM_VDDQ 1.2V 0.0525 TPS54418
      A10_VCCIO_FMCB VCCIO_FMCB & FMCB_VADJ 1.2V 0.0525
      A10_VCCIO_FMCA VCCIO_FMCA & FMCA_VADJ 1.2V 0.0525

    Regards,

    Nicky

    4617.Altera Arria 10 power solutions.pdf

  • Hi Nicky,

    Webench can probably create a discrete solution for you. For PMICs, the TPS65262-2 could supply up to 5 rails, though if used for VCCA_PLL, it would be a bit short of current. Otherwise, the TPS65251 removes the LDOs and provides a bit more current for the bucks.