Other Parts Discussed in Thread: CSD16301Q2, , CSD16406Q3, CSD
Dears,
The BQ29700EVM-610 can support charge current about 5A, and the EVM choose the CSD16301Q2, the MOSFET's Rdson is 23mΩ, If I according the design theory that the max current(VOCD/2*Rdson=100mv/(2*23mΩ)≈2A),I don't konw why can support 5A. Meanwhile, If I want use the BQ29700 to reached 10A discharge current, which MOSFET is the better choice(small size)?
Best Regards
Jacking