Part Number: LM74670-Q1
Other Parts Discussed in Thread: TIDA-00858
Hi,
I see the max input voltage of TIDA-00858 is 42V AC, so, as the Absolute Maximum Ratings in the LM74670 datasheet stated, the 42V from Cathode to Anode(continuous) is actually a AC value? That means the DC value can be 42Vx1.414 (or 45Vx1.414)?
From previous experience, my customer should use 100V diode for the bridge, because 100V is the minimum reverse voltage level that can survive a surge. The AC input range is just 24Vac, but a 3000V peak surge would still remain around 100V after passing a 58V TVS. Could you check if LM74670 can survive a 110V surge with 50us time duration? Any suggestion for this anti-surge design?
Thanks!