This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210-Q1: Device not working at high current

Part Number: TPS40210-Q1
Other Parts Discussed in Thread: TPS40210

Hi,

I am designing a boost converter with TPS40210 part. Specifications are Vi=45V, Vo=60, Iout=700mA.

I used Webench to generate the schematics and choosing the components. Schematics is attached. Now I am trying to test the device for my application. I found that it works fine till 500mA load current and suddenly becomce unstabe after that till 550mA and collepse completely after that. Could anyone please giude me what is wrong with my circuit. I have used most of the compoents as mentioned in schematis. Sense resistor is .05ohm instead of .06ohm. Let me know if any other information is needed. Orrder of capture below is

1. Schematics

2. Stable waveform

3. Unstable waveform

Best Regards,

Rajesh