Hi all
Would you mind if we ask TPS54327?
Please refer to the attachment file.(Vin=12V, Vout=1.5V)
20170418_TPS54327.pdf
Our customer changes the inductor value from 1.5uH to 2.2uH.
In this condtion, when the load changes from 1A to 2A, the switching frequency changes 200kHz upto 800kHz.
Vin and Vout are stable, is it common that the switching frequency changes 200kHz upto 800kHz?
Since there is no internal oscilator, the actual frequency may vary quite a bit.
It depends on "on time".
And then, when the inductor is 1,5uH, when the load changes from 1A to 2A, the switching frequency changes 500kHz upto 800kHz.
We think that this is normal operation.
Kind regards,
Hirotaka Matsumoto