Hi,
considering typical application (figure 27) in the datasheet...I need common ground in the entire circuit, thus I can't use N-FETs. My charger circuit has a shutdown pin (log 0 = shutdown), so my idea is:
- charger circuit connect directly to the akupack
- CHG output connect to the shutdown pin of the charger circuit
- place PFET between AKUPACK+ and LOAD+; use DSG output to connect its gate to the ground via NPN
- between AKUPACK- and LOAD- there will be only the current sense resistor, so what should I do with the LD pin?
I don't mind that there won't be current protection whilst charging (I have it handled in the charger circuit).
Is this a good idea? Will it work? Many thanks