Hello,
My Customer are concerned about switching frequency of boost converter.
They hope to use between 680kHz(min) and 750kHz(max).
Because, In their application, it affects the load as noise by doubling or tripling harmonics(NG 1.6MHz ±5%).
In the datasheets written at 800kHz(min) 1MHz(typ) 1.2MHz(max).
It means , TPS61195 has accuracy of SW frequency about 20%.
Question①
Is there any plan?
Question②
Will the accuracy be higher by reducing the temperature range(0 ~ 45 degrees)?
Vin:4.5~21V
Vout : 40V (12strings, 8parallel)
Iled : 25mA
Regards,
Taichi Nakamura