Other Parts Discussed in Thread: MSP430F5529, , TPS61291, TPS22860, BQ25892
Hi,
Designing a product running from one 700mAh Li-Ion cell. MSP430F5529 and some sensors, device has to wake up every 15 min, take a sample and go back to sleep. Run time is 2 weeks (336 hours). USB connector is provided for charging and data. Power budget for the rest of the system is not set yet.
Looking at the BQ24192 device, it seems that in its lowest power mode it will consume 4mA. This alone yields only 175hrs on a 700mAh pack.
So the next option I have is to use a system timer like a TLP5111 to power everything up, but the BQ24192 seems to lack a 'power off" control signal.
If I could somehow switch off the BQ24192 I would still need a TPS61291 as a boost converter to power the TLP5111 timer to drive a TPS22860 load switch power the BQ24192.... which is just messy.
Does anyone know of a device like a BQ24192 that would be more suitable for use as a Li-Ion battery interface in a short term data-logging solution that could be powered off, put to sleep or has an integrated lowIq LDO for a system timer?
Thanks
Stomp!