This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61040: typical circuit for drawing 60mA from TPS61040 + 14.5V & 3.3V IC (common or different) to power the LCD driver and MCU

Part Number: TPS61040
Other Parts Discussed in Thread: TLV61046A, TPS61093, TPS61046

hello.

In one design, using TPS61040, can we draw 60mA from the circuit. if yes please help to suggest the typical circuit for this much current draw.

Specs for the system are -

Vin - 1.8V to 4.2V

Vout - 14.5V

Iout - 50mA to 60mA

Also want to use 14.5V and 3.3V to control the LCD backlight and MCU respectively. Can we use same IC for that or different ones.

Thanks,

Kushang