CIrcuit is based off a web bench design. I added the voltage divider for the enable pin. I can see the ~3.2 volts on the VCC pin but 0V on the output. The enable pin gets above 1.2V. Red layout is the top, blue is the bottom. R6 is 0 so I can experiment with that pin. No difference whether it's populated or not. C5 and C7 are rated for 100V. C1 is rated for 16V. Vout is 0 if no load is connected and I even tried a 5 ohm, 25 W load resistor.
Any thoughts?