Other Parts Discussed in Thread: LP3965
Hello,
In the customer, the inrush current is larger than the short protection current for LP3965 and LP38512.
Please see the following conditions as inrush current.
Is this current acceptable?
<LP38512>
Vout=1.8V or 1.0V
Inrush current, about 3.6A, 0.3ms
Continuous current is about 0.1A
There is no voltage drop in output/input of the device.
<LP3965>
Vout=3.3V
Inrush current, about 6.1A, 0.3ms
Continuous current is about 0.1A
There is no voltage drop in output/input of the device.
Best Regards,
Ryuji