Dear Sir or Madam:
My customer need the "Positive input transient " parameter of TLE4275QKTTRQ1, like below picture:
Can you help?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir or Madam:
My customer need the "Positive input transient " parameter of TLE4275QKTTRQ1, like below picture:
Can you help?
Thanks!
Hi Eric,
TLE4725-Q1 does not have a pulsed Absolute Maximum Rating higher than the DC Absolute Maximum Rating. As such the absoute maximum rating for a positive input transient is 45V. Please keep in mind that this is a stress test only. Applications should be designed to remain within the Recommended Operating range of 42V.
Very Respectfully,
Ryan