Other Parts Discussed in Thread: BQ24617, BQ25700A, BQ24780S
Hello Texas Instruments Specialists,
I am looking for some guidance regarding your battery management chips in particular chips that can charge/balance a 3 cell 11.1V lipo at an output current of around 8-10A. I found a few chips that are capable of charging at 8-10 Amps and can take a large input voltage of about 5-24V such as the BQ24617, but none that seemed to allow the battery to ever so often drain current to a load. In my application I am currently regeneratively charging an 11.1V 1350mAH lipo at a rate of around 8 amps. The battery will most of the time be sitting and charging from a portion of the 8 amps produced, though at other times the same generator producing the 8 amps of power may want the battery to drain 10-20A to it to start. This is essentially a two way system where at very short periods the lipo battery will be providing power and at longer periods it will be charging/balancing. I am hoping I could get help in finding a chip capable of balancing and charging as well as allowing the current to flow in the opposite direction to the input. I would also greatly appreciate advice towards other options if possible such as storing the 8 amps of power instead of forcing it to the battery.
Thank you,
Tarik