This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31710X2EVM: LMZ31710X2EVM

Part Number: LMZ31710X2EVM

I am testing the LMZ313710X2 evaluation board.

I have a issue measuring the correct current across the sense resistors of 1mOhm (R9,R10).

I am using HAMEG HM7042 power supply to supply input voltage of 12V, I set the output voltage via jumper to 1.8V.

I am feeding a external clock input of 300kHz to synchronize two devices on the evaluation board.

I should be reading across the 1mOhm resistor arnd ~8mV-9mV using DMM but get 0 on both devices.

Is there something I am missing tosetup or add for correct operation and test to get desired output currents from devices?

Please advise

Thanks