Two questions:
1: Is the only difference between the TLC59025 and the TLC5925 the matching of the ourput currents?
2: What happens if you set the current at such a level that the product of current and load impedance is higher that the avaliable voltage, e.g.
If I set the current at 20mA , connect my load that has an impedance of 500Ohms at 5Vcc.
Will the driver saturate at 0.4V and deliver no more than ~9.2mA but stay stable (no oscillations)?
Reason I am asking is that I want to combine driving 7 LEDs, that need 20mA constant current and 8 Reed relais that are 500Ohms but need 5V drive voltage.
Using the unused outputs of the TLC5925 to power the reed relais saves me additional drive logic.
Will the TLC5925 be able to drive an inductive load?