Other Parts Discussed in Thread: TPS3898, , TPS3896, TPS3895, TPS3897
Hi everyone,
I'm trying to use the TPS3895A (SENS_OUT: active high) in order to detect low voltage in a voltage input of 12 Volts. My Theoretical Vtarget is 9 Volts, so with R1 = 500K and R2 = 30K Vtarget = 8.83 volts.
I've read in the datahseet that Vsens <= 6.5Volts. In my case Vsens = R2/(R1+R2) * 12 = 30 / 530 *12 = 0.6792 Volts
But I was reading the document: User's Guide - SLVU524A–August 2011–Revised September 2011 - TPS389xA-xP-EVM047 Evaluation Modules and it seems to be that the maximum voltage in the Jp pin is 6.5Volts:
Does anyone know if my configuration is right? or I can't use an input of 12 Volts in the resistance network (R1/R2).
Best regards.