Other Parts Discussed in Thread: TPS61178, TPS61089, TPS61088
Hi,
So I have here the EVM for the TPS61178. The device is rated to handle voltages as low as 2.7V but the EVM is optimized for
inputs 5V to 12V and a fixed output of 16V.
I changed the feedback resistor Rupper value from 1000k to 600k, to get the output voltage to be around 10.2V.
I'm working with a lithium ion battery rated at 3.7V nominal, 2400mA. I will pull at max around 0.7A - 1A from the battery. The load
is a class-D amplifier connected to two speakers ( 8 ohms each), so the current draw will be very dynamic.
Is it okay for me to work with a voltage this low for this EVM (3V to 4V) ?
Thanks,
Nabil