Part Number: BQ25071-Q1
Other Parts Discussed in Thread: BQ25071
Hi
I have two questions on the LifePo4 precharge current :
-What is the real voltage value (min / typ / max) considered in the BQ25071 for the precharge current for LiFePo4?
-What is the time out value ( min / typ / max) considered in BQ25071?
Can you confirm that the _CHG indicator will go high impedance if the time out has elapsed and the battery voltage is still under the pre-charge threshold of 0.7V (+/-0.2V)?
Thanks and regards,
Mohamed