Other Parts Discussed in Thread: UCC27512
Hello team,
I noticed the UCC27511 datasheet abs max rating table, the OUTH has only indicate DC is -0.3V but no pulse spec, and OUTL has -2V for pulse spec, can you tell why?
When if negative pulse -1.5V happens at OUTL pin, then should be at OUTH present the almost same pulse because R1 and R2 are low impedance.
So, only OUTL can support -2V has no help, OUTH should be support -2V as well.
Right now my customer happens UCC27511 FA issue, I would need to check pin waveform, please comment about my question, I need your help to explain the abs max rating about this.
Thanks a lot.
Martin