Hi,
I wish to track the maximum power of Thermoelectric Generator(TEG).(Voc=17V I=200mA) The output is connected with an Electronic Load。
First,I connected the Thermoelectric Generator(TEG) with Electronic Load directly。I changed the resistance value of Electronic Load (it worked at constant resistance mode),and found that the maximum output power of TEG was 2.42W,the value of resistance was about 40Ω。
Then ,I connected the TEG with the input of the SM72445EVM。The output of the EVM was connected with Electronic Load。When Electronic Load worked at constant voltage mode,the EVM can not enter MPPT mode until the load voltage was below 7V。In MPPT mode the load power changed rapidly,and can just approach 1.05W; When Electronic Load worked at constant resistance mode,the EVM can not eater MPPT mode until the load resistance is about 20Ω.The load can not approach the ideal power。I want to know why,and how can I use this EVM?
Thanks for your help. This project is very important for me
Shuo Wang