Other Parts Discussed in Thread: BQ27350
Hello.
I have a couple of questions relating to the bq27350. I have a 4P pack of 18650 Li ion cells, capacity approx 8Ahr and I am charging to 4.1Volts. I am creating the golden pack on an assembled battery pack. I have followed the procedure in application note "Data Flash Programming and Calibrating the bq27350 Gas Gauge" section 2.1 Creating Pre-Learned Defaults. Qmax did not update after the first full discharge (step 9), but it did update after a subsequent full charge, and Update Status is now set to 06.
I decided to do a couple more charge and discharge cycles to improve the accuracy of the Ra values, however I have found that the RUP_DIS bit has been set and now the Ra table is not updating. Is this normal or does this indicate a problem with the Ra table and Qmax values?
Secondly, the above application note mentions in step 11 when exporting the .gg file, to edit the file and change Update Status to 00. If I load the file into a production battery pack and enable the IT algorithm, then the Update Status bit becomes 04. Does this mean that all production batteries in the field will require to go through a learning cycle in order for the Update Status bit to change to 06? I understand that prior to the first Qmax update, you have to pass > 90% capacity before Qmax will update. I am concerned about this because in the field, our device will rarely discharge completely and therefore it is possible that this learning cycle will never occur.
The last question I have is regarding the FC bit. It is likely that we will have some chargers that will stop charging before the current reaches the Taper Current value. In this case the FC bit will not be set and the fuel gauge does not realise that the battery is fully charged. Will this cause problems with the future accuracy of the fuel gauge as the battery ages?
Thanks and regards,
Jenny