This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF6025: REF6025

Part Number: REF6025

Dear Sir, please, answer

I'd like to use REF6025 for voltage control  of  Voltage Control Oscillator JT53LV (16 MHz) . Oscillator has control input for feed 1.5 V+/- 1V voltage. I want to adjust this voltage with a potentiometer, the voltage from the REF6025 will be applied to the potentiometer, and from potentiometer - to VCO. Temperature range: minus 40 to plus 60 C.

QUESTION: Can I use C load cap (see item 9.3.4 of REF6025 datasheet) ceramic 10 microF - GRM188R60J106ME84 ?  I do not care what kind of capacitor to put, but I can not figure out how to choose the ESR. The required value of ESR is too small to select a suitable capacitor. 

TIA.

Sincerely,

Vladimir Naumenkov

www.agat.by