Other Parts Discussed in Thread: BQ2002E, , BQ27210, BQ34Z100-G1, BQ34110, BQ34Z100, BQSTUDIO
Hello,
My local TI sales rep has been working with the Battery Management Group to find a gas gauge solution for a 2-cell NiMH device I have. To date, it looks like the BQ27220 + TPS61098x boost DC:DC is the best solution. We already use the BQ2002E for the NiMH charging system, have been for years. In my application, the BQ27220 will be on the "system" side. The TPS61098x will get its power from a diode-or'd configured 3.3V and NiMH battery voltage. I understand that I am using the BQ27220 only as a coulomb counter. I have a few questions regarding operation.
1. I'm assuming that TI's recommendation to use the BQ27220 (intended to Li-Ion cells) will work as a coulomb counter in our 2-NiMH configuration, correct?
2. Since we are using the BQ27220 in the "system" side, can the chip operate as intended if we don't use the OTP Flash and just use RAM for battery profiling?
3. The register set of the BQ27220 looks much like the BQ27210. All coulomb data is read-only and data is not restorable should 3.3V go to 0V and the battery voltage down to 1.8V. This will mandate the use of a boost converter in order to retain coulomb data (TPS61xxx).
4. In the register table (page 16 of SLUUBD4), states that the TEMP register is R/W and the ARTTE register is RO. In the BQ27210, TEMP is RO and ARTTE is R/W. I'd assume that SLUUBD4 is incorrect.
5. Like the BQ27210, the BQ27220 is going to be in production for at least 5 more years, correct?
6. Is there any protection for the BAT, SRP, SRN pins should the batteries be put in backwards (or TI recommended external protection)? The TPS61xxx DC:DC boost is protected since the battery voltage and 3.3V are diode-or'd.
- It appears that only the BAT pin will need protection if SRP and SRN are used for lo-side current sensing (see datasheet, page 12).
- Should BAT be connected to the 3.3V input instead of + of the battery? I know that the battery voltage (VOLT register) will always read 3.3V.
Thanks,
...kevin braun