Other Parts Discussed in Thread: LM25011
Hello,
I have some issues with my prototype board.
Iam using LM25011 reference design more or less, 2A load @5V.
I supply the circuit with 12V from and ideal power supply. But I measure 13V and the small ripple. On the output I get 1.5V with a small load. And when I measure the SW node I see its not swithing.
Have I missed something? Just ordered a EVAL board with more or less the same design to compare.
But does anyone have any good reason of the behavior?
I can provide with pictures of the result of that is interesting.
Thanks in advance.