Input Voltage Range:
The TPS53015 switching controller datasheet lists an input voltage range of 4.5V to 28V.
The evaluation module for this IC, TPS53015EVM-126, lists an input voltage range of 8V to 22V.
Does anyone know why these are different?
Output Voltage Range:
The output voltage range of the TPS53015 is adjustable (0.77V to 7.0V) based on voltage divider values at VFB pin (datasheet p15). I'm assuming that I can change these resistor values on the EVM in order to change the output voltage (Default Vout is 1.05V). Is it possible that the Vin range on the EVM is set in order to meet this output range?
Basically, I would like to use the EVM for 5Vin and 3Vout. Would like to make sure it can do this before I purchase.