This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43061EVM-198: TPS43061EVM-198 5Volts to 12Volts -right?

Part Number: TPS43061EVM-198

 Hi!
About TPS43061EVM-198:
I made a search for up-stepper / booster Vin 5 Vout 12 and got that suggestion from the ti-website.
In the discription it say's: "The EVM operates from a 6V to 12.6V input (9V nominal) and provides a 15V output at 2A."
I could succes a search up to 13,4 Aout.
Something is wrong here...
The search-results tells one thing, discription an other.
If i connect 5Volts to a TPS43061EVM-198 (and enough Amperes) -would it give me 12V and 13,4A out?
...or have i made some kind of missunderstanding?

Thank you!