Other Parts Discussed in Thread: TPS2500, , TPS63060, TPS63000, TPS62170, TPS63050, TPS62750
Hello Community!
Im interested on how to properly make use of an protected usb power supply.
The device i am developing is going to be supplied by a usb port of an computer/laptop.
So far i know laptops have an 5V-500mA output.
What i actually want to do stabalize and boost my incomming voltage supply from the laptop to 5V 500mA and 3V3 500mA (i prefer more amps. but as far i've calculated i need atleast in total of 350 mA.
I've found something like the TPS61092 or TPS2500?
But then i read something about atleast 1A input?
Would i need to use of an buck/boost converter? Or can i just take the input of an laptop?
And what about surge-protection?
Can you guys help me out on how to go to the next step?
Best regards,
Klaas