I am facing an issue with the LM3409 driver. This buck regulator is not working. It just passes the input voltage (24V) to output.
Design Specification(I have Attached a Schematic)
Vin:24V,
Vout : 12V
Current: 1.2A
I used a dimming through adjusting the voltage at Iadj pin. Initially, i have connected the Enable Pin to 24V, later i have kept open. It does not have any effect on working of driver
As I have connected one Led strip(4 LEDs in series, Vf -3V/Led), so led strip should be ON as per design.but It is not working as output is 24V instead of 12V, so i have connected 2 Led strips in series and its working
also dimming of Leds are working very well.
My problem is that, as per design specification output should be 12V.
I might be missing something obvious.
Any ideas on how to troubleshoot this would be very helpful.
Thank You.leddriverlm3409.pdf