Part Number: BQ51221
Other Parts Discussed in Thread: BQ51021
In the datasheet I2C section (page 7), the test conditions stated pull-up voltage = 1.8V and the abs. max. ratings (page 4) = +7V.
Is it safe to use +5V pull-up for normal operation?
If so, I assume, the threshold would still be +0.4V & +1.4V?
Would the same answer apply to BQ51021 (bq51221-EVM & BQ51021 product) ?
Thank you,