Part Number: LM25066A
Hello,
I am implementing an additional circuit that provides external current (~80uA) to the TIMER capacitor on my LM25066A to speed up the insertion time, but not affect the fault timing. When my circuit is powered on and the LM25066A does not have any input voltage (LM25066A is powered off), my circuit applies ~1.5V to the TIMER pin. Is this safe for the LM25066A? As soon as the input voltage reaches the POR, my circuit works as expected.
Please let me know if it is safe to have external voltage applied at the TIMER pin when the LM25066A is powered off. If so, how high can the voltage be?
Thanks,
Chris