Other Parts Discussed in Thread: TPS61291, TPS610981, TPS61099, TLV61220
Hello I have an application where I will be running from 2 AAA batteries and need to generate a 3.3V Output. The TPS61070 looks to be an idea part for this. I had a couple of questions regarding this device.
It is a BLE Beacon application in which the typical average current will be ~15-20uA. It will Transmit every ~2seconds with a Peak Current of ~5-6mA. In between Transmits it will be in a Low Power mode ~2uA. My biggest concern is the operation at these low load levels.
1) The 61070 has the Power Save Mode which indicates that at Low Loads it produces several pulses to keep a desired Vout. What I am not clear on is the Efficiency Graph shows essentially 0% efficiency down at these low load levels? Should I be concerned about this or is this just a byproduct of how the Power Save mode works? I.E. - I would have thought the efficiency would still be relatively good in this Power Save Mode.
2) Do you have any data on efficiencies for the TPS61070 with a Vin ~3V (2 AAA's at full capacity) with a Vout = 3.3V? The graphs only show 2.4V as the highest input voltage.
3) The device will have an ON/OFF switch in which the BLE device will detect a Long Press on the Pushbutton to drive the EN line Low on the TPS61070. While the TPS61070 provides the ability to disconnect the Load from the Battery I am not seeing that it provides the capability to discharge the Output Cap, possibly I have missed this. If this is the case and the system enters a very low power mode <1uA a fully charged Output cap could take some time to discharge to where the system truly is shutdown. Do you have a recommendation on how to discharge the Output cap when the EN line is driven low and that won't cause additional drain during normal operation? I had thought of just using a N-FET that could be turned on when EN goes low to connect the Output Cap to a discharge Resistor. I could even use a P-N FET combo in which when the EN line goes low this turns on the P-FET supplying the Gate of the N-FET with Vout turning on the N-FET that connects the Output cap to the discharge resistor to GND.
Thoughts?
Regards,
Frank