This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61028: pawer save mode

Part Number: TPS61028
Other Parts Discussed in Thread: TPS61098

HI,

I am checking the power save mode of TPS 61028.
For continuous mode and power save mode, the timing of the behavior of
these two modes is changed, what kind of conditions are there?
Is the output current lowered and the inductor current become discontinuous operation?

(specification)
VIN: 1 V to 3 V
VOUT: 2.8 V
IOUT: max 100 mA, the standby current is under consideration

Best Regards,