This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030-Q1: LMR14030-Q1 3.3V 2MHz solution

Part Number: LMR14030-Q1

LMR14030-Q1 can be used under the following conditions?

 If possible, Please tell me the recommended circuit (especially Schottky diode).


◆Condition


Vin:6~16V


Vout:3.3V


Iout:3.5A max


Fsw:2MHz (Above AM band)

Regards

Tomohiro Nagasawa