This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2825: Setting the frequency value of UC2825

Part Number: UC2825

Hi

My customer will set the Freq=130kHz(Rt=7.5kHz, Ct=2200pF).

Please let me confrim the attached figure just to be sure.

  Is this the range of Rt?

②,③

  Could you tell these value(②=5kΩ, ③=500Hz)?

UC2825.pdf

Best regards,

Yokota