Tool/software: WEBENCH® Design Tools
Hi
There is a error in webench regarding the automatic schematic creation of LP38798-ADJ (And possibly the non adjustable too, I haven't checked)
I'm using the following design variables:
VinMin: 14.4V
VinMax: 15.6V
Vout: 13.5V
Iout: 0.2V
In the generated schematic the webench connects the input (VIN) directly to the EN pin. However since there is a zener diode internally this can not be done for voltages above 5.5V (As described in the datasheet of the LP38798). VIN in my case is way above 5.5V
The webench application should've not put any connection to the EN pin because its internally pulled up or should put a 2Mohm resistor between VIN and EN to lower the power to about 7.5uA
Just letting someone of Ti know to change this, cheers!