Hi
UCC25630 can be used for LLC, and can use UCC25630 for LCC applications or not ?
thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
UCC25630 can be used for LLC, and can use UCC25630 for LCC applications or not ?
thanks,
Hi Jerry,
Yes, you can use UCC25630 for LCC applications.
Best Regards,
Ben Lough
Hi Benjamin,
The voltage of the resonant capacitor is used to realize the HHC control, which is well implemented in the LLC. The voltage of the resonant capacitor reflects the input current status very well, and the loop is controlled by the VCR pin. If we use the LCC topology, how can we implement the HHC loop control, and VCR take the voltage of the shunt capacitor (ripple is small), and the resonant capacitor voltage has been clamped by output , Our problem is how to take VCR signals without sacrificing HHC performance too much. Our switching frequency should be above 500KHZ. What are the problems we need to consider ? Are specifications in page 17, formula 2, page 22, and the descriptions between figure 34 and figure 33 incorrect ? Thank you.
Hi Jerry,
You can choose the capacitor divider such that the sign on VCR pin is big enough, but not exceed the 0-6V range. You need also make sure the capacitor used in the divider is much smaller than the resonant capacitor.
Regards,
Bosheng