This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34925: LM34925

Part Number: LM34925
Other Parts Discussed in Thread: LM5160

Dear sir,

In the above mentioned part number that is LM34925 (Isolated DC-DC Converter),

  1. Can we use only single output (VOUT2), by making VOUT1 as dummy ?
  2. Since the minimum input voltage for LM34925 is 7.5V , what  happens at the output if the IC(LM34925) receives below the min input voltage (Ex is ,if suppose the input voltage is 5V) ?
  3. Is it possible to tune the output voltages by resistor ?

Awaiting for your kind replays

Thanks 

Hemantha Kumara N K