Part Number: LM34925
Other Parts Discussed in Thread: LM5160
Dear sir,
In the above mentioned part number that is LM34925 (Isolated DC-DC Converter),
- Can we use only single output (VOUT2), by making VOUT1 as dummy ?
- Since the minimum input voltage for LM34925 is 7.5V , what happens at the output if the IC(LM34925) receives below the min input voltage (Ex is ,if suppose the input voltage is 5V) ?
- Is it possible to tune the output voltages by resistor ?
Awaiting for your kind replays
Thanks
Hemantha Kumara N K