Other Parts Discussed in Thread: BQ25100
We used BQ25100 and BQ29700 in our product.
BQ29700 can cut off the voltage when battery voltage is under 2.8V, so the overdischage protect function is OK.
but we insert a 5V usb for charging and BQ25100 can't charge, battery voltage is 2.83V. it was protected by BQ29700 but why?
I checked the NMOS connect to Cout, the GS voltage(to pack-) is 1.8V, it's high.
the NMOS connect to Dout, the GS voltage is 0V(to VSS), I guess it should be right? but why pack- voltage is higher than VSS so that it can't charge?
the max Vgh th of NMOS is 1.25V.