Because of the Thanksgiving holiday in the U.S., TI E2E design support forum responses may be delayed the week of Nov. 21. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B67-Q1: Body Diode specification

Part Number: TPS7B67-Q1

Hello Team,

my customer is using TPS7B6701 to produce 8V output supply.

This output has to be protected against short to GND and Battery.

A special test will now feed Vbat into output pin without power on input. This means a current is flowing through body diode and activate internal circuits.

Question from customer: Do we specify body diode? This is necessary to calculate worse case scenario and if this diode is able to sustain this test case.

Many Thanks

Josef