Part Number: LM3464
Other Parts Discussed in Thread: LM3553, LM3464, LM3643, LM36010
Support Path: /Product/Help with Device Selection/
I am currently using lm3553 for two IR LEDs flash light.
We are looking to go to 4 LEDs with I2C configuration but there is not many option. If we use the 2 LED driver version for example LM3464 1.5A max, how can we synchronize between two devices?
Maybe we have to use Strobe pin but there is still a delay difference from rising edge of strobe to LED firing across the chip.
Any suggestion?
Thanks
Khoi