Other Parts Discussed in Thread: LM5116, , UCC27511
dear all,
i have made a circuit of buck with following specs,
Vin: 50V,
Vout: 12V, 30A
MOSFET used: CSD19503 as high side mosfet
Driver IC: LM5116,
Gate resistance: 2Ohm
Issue: when testing the schematic with above parameters, my MOSFET gate rise time and fall time are above 100ns.
Datasheet shows Rise time and fall time are 3ns and 2ns. How do i know if the datasheet shows the right parameters or they are just for "sales purpose".
What do i use to make these parameters possible in my schematic. Please suggest.
Vikas Dabas
India