Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24720: TPS24720

Part Number: TPS24720
Other Parts Discussed in Thread: CSD16321Q5, TPS24770

I would like to use TPS24720 design of the largest current 50A with CSD16321Q5 at 12V
How to set  PLIM of  TPS24720, can  you  give a reference design

  • Hi,

    Sorry for the delay,

    Please go to www.ti.com/hotswap to access the excel based design tool, app notes, and video tutorials. In general, the TPS247xx series is used in lower current levels (30A) , but in some cases can be used in higher levels if Cout is not high. The tool will help you determine this. Also recommend you obtain a TI TPS24720 EVM to test prior to design in, modifying it per your system needs. Perform Hot Short, Power Into short tests at max system ambient. If an acceptable solution isn't possible using the tool, consider using the TPS24770. It has a dual timer allowing inrush power up into high capacitive loads and a short fault timer.

    Brian