Hi
As long as I look Fig31 of TLV743's datasheet, I think the maximum power dissipation at Ta=57.9℃ is about 0.29W.
But I calculated the Tj under Pd=0.32W, Tc=72.4℃ and Ta=57.9℃, Tj is 82.5℃.
Could I use this device that condition?
Best regards,
Yokota