Hello.
I have a question.
We configured the power supply using UCC2818A.
We are doing power supply operation test.
UCC2818A stops when we perform the following operation test with the attached circuit.
Why did it stop?
It will not return unless the power is turned on again.
Is there a protection circuit not listed on the data sheet?
Situation
・Environment that works with UCC 2818A alone.
・From RVOUT, flow a 400 mA current using a load device.
・After that, the load device was turned off.
・After that, the UCC2818A stopped its operation after the ON width of DRVOUT changed.
・When stopped, the VREF voltage of UCC2818A is decreasing.
・After that, operation of UCC2818A is restored by turning on the power again.(Latch stop)
In the power supply we created, even when carrying out the noise test, the power supply will stop in the same way.(Latch stop)
Thank you.