Other Parts Discussed in Thread: BQ24161, , BQSTUDIO
I am using the BQ27530-G1 fuel gauge in conjunction with the BQ24161 battery charger. The SYS output of the BQ24161 is connected to a TPS61236 which regulates the system load to 5V. While performing the learning cycle I disconnected the supply input to the BQ24161 so that the system would run from the battery until it reached the fully discharge point. At this point the system begins to cycle on and off which I believe is caused by the battery voltage recovering when the load is removed.
Since this seems like a typical usage scenario where no input is connected and running from the battery that the fuel gauge would disconnect the battery to prevent further discharge. The SysDown Set Volt Threshold is 3150mV, the SysDown Set Volt Time is 2s, the SysDown Clear Volt is 3400mV and the Final Voltage is 3000mV. The IT config has Terminate Voltage as 3000mV, the Term V Delta as 200mV and the ResRelax Time as 500s. The battery is an UltraLife UBBL23 comprised of two 18650 cells in a 1S2P configuration. The total capacity is 4800mAh with a voltage range of 3000mV to 4200mV and a under voltage limit of 2500mV.
Is there a way to configure the BQ27530 to disconnect the internal FET in the BQ24161 so the BAT input is disconnected from the SYS output until a power source is connected to the input of the BQ24161?
Could this be caused by the fact the fuel gauge has not completed the learning cycle?
Thank you.