This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMR16006Y-Q1: LMR16006Y Not showing as an option in Webench, when parameters seem to be within range

Part Number: LMR16006Y-Q1
Other Parts Discussed in Thread: LMR14006

Tool/software: WEBENCH® Design Tools

Gents,

I have a few projects running properly with LMR16006Y, using the fixed 3V3 output version.

Trying to confirm a new design today, but Webench does not see it as a valid option for my parameters:

VIN: 9-36VDC
VOUT: 3.3V
Iout: 300mA
Ambient temp: 50oC

I wonder if this device is actually not suitable for that application? It is automotive rated and should be able to deal with 600mA per the datasheet, on an even wider input range...

Regards

Bruno