Part Number: TPS62410-Q1
Other Parts Discussed in Thread: TPS62410
The TPS62410-Q1 is used in the following configuration.
*The output capacitor (C5) uses "CGA6P1X7R1C226M250AC".
Overshoot was confirmed at VOUT 1 output at power on. (Overshoot of about 240mV)
This overshoot does not affect the operation.
However, it wants to eliminate the overshoot as for hope.
Q1.
It is possible to increase the output capacitor capacity as a overshoot countermeasure.
Could you tell me if there are other effective measures?
-Harukawa